- HOME
- News
- Press Releases
- 10kW Platform in 2U Height Extends the New Generation Advanced Full-Rack Programmable DC Power Supply Series
10kW Platform in 2U Height Extends the New Generation Advanced Full-Rack Programmable DC Power Supply Series

TDK Corporation announces the introduction of the higher power density 2U Full-Rack 10kW models
Programmable DC Power Supply Series. This expansion now provides the user with 10kW of Output power in a 2U high package and a choice of ten different models (ranging from 10V-1000A to 600V-17.5A) that have advanced performance and functionality well suited for Laboratory/R&D, Design and Test & Measurement environments and address broad market segments including Automotive, Aerospace, Semiconductor, Industrial and Renewable/Alternative Energy.
Built into a lightweight 3U high, 19” (483mm) wide rack-mountable chassis, the 3U Full-Rack 10kW DC Programmable Power Supply Series offers five embedded front panel setup menus that address Digital Communication, Protective Functions, Operating Configuration, System Configuration, and System Triggering. These embedded menus offer user-selectable functions including Internal Resistance simulation and Slew-Rate control of Output voltage/current and have the capability to generate, store, recall and activate up to four on-board Arbitrary waveform profiles.
All models can operate in Constant-Current (CC), Constant-Voltage (CV) as well as the newly offered Constant-Power (CP) limit and have conversion efficiencies up to 92%. Three-phase AC Input options include 208VAC (170~265VAC) or a wide-range 400VAC/480VAC (342~528VAC) and have built-in active Power Factor Correction (0.94 typical) with cooling fan speed control (for reduced audible noise and extended life).
Standard safety features include user-selectable Safe-Start/Auto Re-Start and Last Setting Memory along with other built-in protective functions that include Output Over-Voltage Protection (OVP), Output Under-Voltage Limit (UVL), Output Under-Voltage Protection (UVP), Fold-Back protection (FOLD) for CV or CC mode, Output Over-Current Limit (OCL) and Over-Temperature protection (OTP).
All model functions can be programmed locally via the menu-driven front panel display or remotely using software instrument drivers with any one of the three built-in standard Digital interfaces (LAN (LXI 1.5), USB (2.0) and RS-232/RS-485). Other programming interfaces include the built-in standard 5V/10V Isolated Analog Program/Monitor/Control Interface and the optional IEEE (IEEE 488.2 & SCPI compliant) Digital interface.
The 3U 10kW Power Supply Series carries a five (5) year warranty, has Safety certifications to IEC/EN/UL/cUL 60950-1 and is CE marked in accordance with the Low Voltage, EMC (IEC/EN61204-3; industrial environment) and RoHS2 Directives.
More information can be obtained at the following TDK-Lambda Americas website, https://www.us.lambda.tdk.com/products/programmable-power/genesys-plus.html, or by calling 800-LAMBDA-4.
About TDK Corporation
TDK Corporation is a leading electronics company based in Tokyo, Japan. It was established in 1935 to commercialize ferrite, a key material in electronic and magnetic products. TDK's portfolio includes electronic components, modules and systems* which are marketed under the product brands TDK and EPCOS, power supplies, magnetic application products as well as energy devices, flash memory application devices, and others. TDK focuses on demanding markets in the areas of information and communication technology and consumer, automotive and industrial electronics. The company has a network of design and manufacturing locations and sales offices in Asia, Europe, and in North and South America. In fiscal 2018, TDK posted total sales of USD 12 billion and employed about 103,000 people worldwide.
About TDK-Lambda Corporation
TDK-Lambda Corporation, a group company of TDK Corporation, is a leading global power supply company providing highly reliable power supplies for industrial equipment worldwide. TDK-Lambda Corporation meets the various needs of customers with our entire range of activities, from research and development through to manufacturing, sales, and service with bases in five key areas, covering Japan, Europe, America, China, and Asia.
For more details, please pay a visit to https://www.tdk-lambda.com/
Contacts for Regional Media
| Region | Contact | Phone | |
|---|---|---|---|
| Americas | Tom Goodman
Product Manager Low Voltage Products |
+1 732 795 4148 | tom.goodman@us.tdk-lambda.com |