TDK-Lambda Americas Blog

Class 2 or Class II power supplies?

60950-1 Class I & II Class 1 & 2 Safety Certification

May 23, 2011

One question I am frequently asked is: “The customer is looking for a Class two power supply; what can you offer him?”

My response is always “Class 2” or “Class II (with Roman numerals)”, or both? The pause on the end of the phone signifies an explanation is in order.

Class 2

Class 2 is a classification referring to the NEC – National Electric Code. To avoid potential cable overheating due to excessive currents and electric shock, the output of the power supply is limited to 60VDC or 100VA, (100W when used with an AC-DC power supply). You will often see 24V output DIN rail power supplies or LED drivers rated at 91W rather than 100W because if the power supply is overloaded, any tolerance in the over current protection has to be accounted for.

Often these products will be certified to UL1310 and will list this in the datasheet. An example of this is TDK-Lambda’s DSP Series. You can see from the model selector list on page 2 of the DSP datasheet that output currents of 4.2A or greater are not approved to UL1310.

Class II

Class II (with Roman numerals) refers to power supplies with either a double or reinforced insulation barrier between the input and the output. Class II supplies do not rely on an earth connection to protect against shock hazard. Many cell phone chargers and laptop power supplies are Class II. TDK-Lambda’s DSP series also are Class II, having just a Line and Neutral AC input without a ground connection.

A Class II power supply rating label will show this symbol:

2011-05-fig1.gif

One advantage of Class II is better surge protection between input and ground and usually a lower earth leakage current.

For more information about leakage current, please see another article about power supply leakage current testing.

Power Guy

Social Media

PAGE TOP