- HOME
- News
- Press Releases
- OVC III certified 600W half-brick power module operates from a 200 to 425Vdc input
OVC III certified 600W half-brick power module operates from a 200 to 425Vdc input

San Diego, CA - April 16, 2020
TDK Corporation (TSE 6762) announces the introduction of the TDK-Lambda PH600A280-24 DC-DC converter. Rated at 24V 600W, this further extends the 280Vdc nominal input PH-A series from 50W to 600W. The PH-A series is utilized in HVDC (High Voltage Direct Current) equipment for data communications, high voltage transmission, renewable energy applications, robot controllers and factory automation.
Certification to the safety standard EN 62477-1 (Over Voltage Category III) benefits users requiring compliance to the machinery safety standard IEC 60204-1. The PH600A280 does not require an isolation transformer on the distribution panel, reducing cost, size and weight.
The PH600A280-24 accepts a wide range 200 to 425Vdc input delivering 24V at 12.5A. The output voltage can be set between 14.4 and 28.8V using the trim terminal. With an efficiency of 93%, the module can operate at full load with baseplate temperatures of -40°C to +85°C, derating linearly to 80% load at +100°C. Conduction cooling through the baseplate enables the PH-A to be used in outdoor sealed enclosures or liquid cooled equipment.
Following the industry standard, the half-brick package measures 61.0 x 12.7 x 57.9mm (WxHxL). The PH600-A has remote on-off, over-current and over-voltage protection and a five-year warranty. Input to output isolation is 3,000Vac and is safety certified to IEC/EN/UL/CSA 62368-1, EN 62477-1 (OVC III) with CE marking for the Low Voltage and RoHS Directives.
More information can be obtained on the TDK Product Center, or by calling 800-LAMBDA-4.
Major Applications
Data communications, high voltage transmission, renewable energy applications, robot controllers and factory automation
Main Features and Benefits
- • Very compact half-brick package
- • Up to 93% efficient
- • Baseplate cooled
- • -40 to 100°C baseplate temperature range
- • Certified to EN62477-1 (OVC III)
Key Data

About TDK Corporation
TDK Corporation is a leading electronics company based in Tokyo, Japan. It was established in 1935 to commercialize ferrite, a key material in electronic and magnetic products. TDK's comprehensive portfolio features passive components such as ceramic, aluminum electrolytic and film capacitors, as well as magnetics, high-frequency, and piezo and protection devices. The product spectrum also includes sensors and sensor systems such as temperature and pressure, magnetic, and MEMS sensors. In addition, TDK provides power supplies and energy devices, magnetic heads and more. These products are marketed under the product brands TDK, EPCOS, InvenSense, Micronas, Tronics and TDK-Lambda. TDK focuses on demanding markets in the areas of information and communication technology and automotive, industrial and consumer electronics. The company has a network of design and manufacturing locations and sales offices in Asia, Europe, and in North and South America. In fiscal 2019, TDK posted total sales of USD 12.5 billion and employed about 105,000 people worldwide.
About TDK-Lambda Corporation
TDK-Lambda Corporation, a group company of TDK Corporation, is a trusted, innovative leader and global supplier of highly reliable power conversion products for industrial and medical equipment worldwide. TDK-Lambda Corporation is aligned for fast responses to any customer need with R&D, manufacturing, sales and service locations in five key geographic regions, namely Japan, EMEA, Americas, China and ASEAN.
For more details, please pay a visit to www.jp.lambda.tdk.com/en/
Downloads
Editorial Contact
- Tom Tillman, Director of Marketing
- TDK-Lambda Americas Inc.
- 401 Mile of Cars Way, Suite 325
- National City, CA 91950
- Ph: 619-575-4400
- Email: mailto:tom.tillman@us.tdk-lambda.com