- HOME
- News
- Press Releases
- Advanced 1U Full-Rack AC/DC Programmable Power Supply Series Continues to Grow with the Addition of a 3.4kW Platform
Advanced 1U Full-Rack AC/DC Programmable Power Supply Series Continues to Grow with the Addition of a 3.4kW Platform

Neptune, NJ - November 2019
TDK Corporation (TSE 6762) announces the introduction of the TDK-Lambda 1U Full-Rack GENESYS+™ 3.4kW AC/DC Programmable Power Supply Series. Adding to the already released 1.7kW, 5kW, 10kW and 15kW platforms and the just released 2.7kW platform, the 3.4kW platform provides the user with a choice of ten different models, ranging from 10V-340A to 600V-5.6A, that have advanced performance and functionality well suited for Design, Test and Measurement within the Laboratory/R&D environment and address broad market segments including Automotive, Aerospace, Semiconductor, Industrial and Renewable/Alternative Energy.
Built into a lightweight 1U high, 19” (483mm) wide rack-mountable chassis, the GENESYS+™ 3.4kW Power Supply Series offers five embedded front panel setup menus that offer user-selectable functions including Internal Resistance simulation, Slew-Rate control of Output voltage/current, Constant-Power limit and Arbitrary waveform generation.
All models have three AC Input options which include a single-phase 230VAC Input (with 0.99 PF), a three-phase 208VAC Input (with 0.94 PF) or a wide-range 400VAC/480VAC Input (with 0.94 PF), and have conversion efficiencies up to 90.5% with cooling fan speed control (for reduced audible noise and extended life).
Standard safety features include user-selectable Safe-Start/Auto Re-Start and Last Setting Memory along with other built-in protective functions including Output Over-Voltage Protection (OVP), Output Under-Voltage Limit (UVL), Output Under-Voltage Protection (UVP), Fold-Back protection (FOLD) for CV or CC mode, Output Over-Current Limit (OCL) and Over-Temperature protection (OTP).
A new Advanced Parallel Master/Slave system allows for up to four units to be connected in parallel with Auto-Configuring technology and provides dynamic response and Output voltage ripple/noise characteristics comparable to that of a single unit.
All model functions can be programmed locally via the menu-driven front panel display or remotely using software instrument drivers with any one of the three built-in standard Digital interfaces (LAN (LXI 1.5), USB (2.0) and RS-232/RS-485). Other programming interfaces include the built-in standard Isolated Analog Program/Monitor/Control Interface, the optional IEEE (IEEE 488.2) and ModBUS-TCP Digital interfaces.
The GENESYS+™ 3.4kW Power Supply Series carries a five (5) year warranty, has Safety certifications to IEC/EN/UL/cUL 60950-1 and has CE marking in accordance with the Low Voltage, EMC (IEC/EN61204-3; industrial environment) and RoHS Directives.
More information can be obtained on the TDK Product Center, or by calling 800-LAMBDA-4.
About TDK Corporation
TDK Corporation is a leading electronics company based in Tokyo, Japan. It was established in 1935 to commercialize ferrite, a key material in electronic and magnetic products. TDK’s portfolio features passive components such as ceramic, aluminum electrolytic and film capacitors, and magnetics, high-frequency, and piezo and protection devices. The product spectrum also includes sensors and sensor systems such as temperature and pressure, magnetic, and MEMS sensors. In addition, TDK provides power supplies and energy devices, magnetic heads and more. These products are marketed under the product brands TDK, EPCOS, InvenSense, Micronas, Tronics and TDK-Lambda. TDK focuses on demanding markets in the areas of information and communication technology and automotive, industrial and consumer electronics. The company has a network of design and manufacturing locations and sales offices in Asia, Europe, and in North and South America. In fiscal 2019, TDK posted total sales of USD 12.5 billion and employed about 105,000 people worldwide.
About TDK-Lambda Corporation
TDK-Lambda Corporation, a group company of TDK Corporation, is a leading global power supply company providing highly reliable power supplies for industrial equipment worldwide. TDK-Lambda Corporation meets the various needs of customers with our entire range of activities, from research and development through to manufacturing, sales, and service with bases in five key areas, covering Japan, Europe, America, China, and Asia.
For more details, please pay a visit to http://www.tdk-lambda.com
Downloads
Editorial Contact
- Tom Goodman
- Product Manager, Low Voltage Products
- TDK-Lambda Americas Inc.
- 405 Essex Road
- Neptune, NJ 07753
- Ph: 732-795-4148
- Email: tom.goodman@us.tdk-lambda.com