- HOME
- News
- Press Releases
- New Generation Full-Rack 1U AC/DC Programmable Power Supply Series Extended with Five New Output Configurations
New Generation Full-Rack 1U AC/DC Programmable Power Supply Series Extended with Five New Output Configurations
San Diego, CA – October, 2018 -
TDK Corporation announces the introduction of five new models to the TDK-Lambda high power density 1U Full-Rack
5kW AC/DC Programmable Power Supply Series. This model expansion includes the 40V, 60V, 80V, 100V and 150V models and now provides the user with a choice of ten different models ranging from 10V/500A to 600V/8.5A.
Launched in 2017, the
5kW Series utilizes embedded microprocessor technology and provides advanced performance and functionality well suited for Design, Test and Measurement in the Laboratory/R&D environment and addresses broad market segments including Automotive, Aerospace, Semiconductor, Industrial and Renewable/Alternative Energy.
This air-cooled product, which is the first to be offered in a new generation platform, brings a higher level of performance to the TDK-Lambda AC/DC Programmable Power Supply product portfolio at a competitive price and is functionally compatible with the comprehensive TDK-Lambda Genesys™ Series.
Carrying a five (5) year warranty and built into a 1U (1.75”) high, 19” (483mm) wide, and 17.5” (444.5mm) deep rack-mount mechanical profile, the
5kW Power Supply Series offers the highest power density (35% higher) and, at 15.4lbs (7kg), the lightest weight in the industry (less than half that of comparable products).
Ten models are now currently available from 10V to 600V with outputs of 10V/500A, 20V/250A, 30V/170A, 40V/125A, 60V/85A, 80V/65A, 100V/50A, 150V/34A, 300V/17A and 600V/8.5A with conversion efficiencies up to 92%. These units can operate in Constant-Current (CC), Constant-Voltage (CV) as well as the newly offered Constant-Power (CP) limit. Three-phase AC Input options include 208VAC (170~265VAC), 400VAC (342~460VAC) or a wide-range 480VAC (342~528VAC) and have built-in active Power Factor Correction (0.94 typical) with cooling fan speed control (for reduced audible noise and extended life).
In addition to doubling the power density over the existing 2U Genesys™ 5kW Programmable Power Supply Series, the
5kW platform offers other significant advancements. These include a high contrast, wide viewing angle multi-segment front panel LCD display (with user controllable brightness and dimming functions for improved readability) that has five embedded multi-functional Power Supply Setup menus that address Digital Communication, Protective Functions, Operating Configuration, System Configuration, and System Triggering. These embedded menus offer new adjustable user-selectable functions including Internal Resistance simulation, Constant-Power limit and Slew-Rate control of Output Voltage/Current. Arbitrary waveform profiles, such as vehicle battery start-up simulation, of up to 100 steps can also be generated and stored in four on-board memory cells and can be recalled and activated via the front panel display embedded menus or Remote Digital communication.
Standard safety features include user-selectable Safe-Start/Auto Re-Start, Last Setting Memory and various built-in protective functions. With Safe-Start configured, the power supply returns to its last operational settings after a power interruption but with the output disabled. With Auto Re-Start, the power supply returns to the last used operation settings after a power interruption. Last Setting Memory retains settings such as the Output voltage/current, Output ON/OFF, Output OVP/UVL/UVP level, Fold-Back (CV or CC), Output Over-Current Limit (OCL) and Start-Up mode (SAFE or AUTO) at each AC input turn-off sequence. Built-in protective functions include Output Over-Voltage Protection (OVP), Output Under-Voltage Limit (UVL), Output Under-Voltage Protection (UVP), Fold-Back protection (FOLD) for CV or CC mode, Output Over-Current Limit (OCL) and Over-Temperature protection (OTP).
A new Advanced Parallel Master/Slave system, unique to TDK-Lambda, allows for improved multi-unit system performance (Output ripple/noise and dynamic response) where up to four
units can be connected in parallel and automatically configured by detection of the parallel data-link cable connections between units, with the Master unit being the single point for programming, measurement and status of system load current.
All model functions can be programmed locally via the menu-driven front panel display or remotely using one of the three built-in standard SCPI-compliant Multi-Drop Remote Digital communication interfaces (where up to 31 units may be controlled in an addressed RS-485 Multi-Drop configuration). These standard interfaces include the LAN ( 1.5), USB (2.0) and RS-232/RS-485 (115.2kBaud) and an optional SCPI-compliant Multi-Drop GPIB (IEEE 488.2) Remote Digital communication interface (all of whose communication protocols and signals are compatible with the entire TDK-Lambda Genesys™ Series). Also included is a full selection of software instrument drivers, a Waveform-Creator and an Advanced Virtual Front Panel GUI.
A built-in standard Remote Isolated Analog Program/Monitor/Control Interface (with 600V isolation) is also provided with new functions such as Output control pins (for activation of external devices for polarity reversal or load disconnect), Trigger-In/Trigger-Out pins (for synchronization), Enable control (with user-selectable polarity) and higher accuracy Program/Monitor signals.
Two new
mechanical options are a Blank Front Panel and an Air Filter kit. The Blank Front Panel is available for applications where the front panel display and controls are not required and only remote interfacing (Digital/Analog) is needed. The Air Filter kit has a removable snap-in filter (for easy maintenance) and is provided for use in environments where dust is present.
The
5kW Power Supply Series has Safety certifications to IEC/EN/UL/cUL 60950-1 with CE marking in accordance with the Low Voltage, EMC (IEC/EN61204-3; industrial environment) and RoHS2.
More information can be obtained at the following TDK-Lambda Americas website, https://www.us.lambda.tdk.com/products/programmable-power/genesys-plus.html, or by calling 800-LAMBDA-4.
About TDK Corporation
TDK Corporation is a leading electronics company based in Tokyo, Japan. It was established in 1935 to commercialize ferrite, a key material in electronic and magnetic products. TDK's portfolio features passive components such as ceramic, aluminum electrolytic and film capacitors, and magnetics, high-frequency, and piezo and protection devices. The product spectrum also includes sensors and sensor systems such as temperature and pressure, magnetic, and MEMS sensors. In addition, TDK provides power supplies and energy devices, magnetic heads and more. These products are marketed under the product brands TDK, EPCOS, InvenSense, Micronas, Tronics and TDK-Lambda. TDK focuses on demanding markets in the areas of information and communication technology and automotive, industrial and consumer electronics. The company has a network of design and manufacturing locations and sales offices in Asia, Europe, and in North and South America. In fiscal 2018, TDK posted total sales of USD 12 billion and employed about 103,000 people worldwide.
About TDK-Lambda Corporation
TDK-Lambda Corporation, a group company of TDK Corporation, is a leading global power supply company providing highly reliable power supplies for industrial equipment worldwide. TDK-Lambda Corporation meets the various needs of customers with our entire range of activities, from research and development through to manufacturing, sales, and service with bases in five key areas, covering Japan, Europe, America, China, and Asia.
For more details, please pay a visit to http://www.tdk-lambda.com/
Contacts for Regional Media
| Region | Contact | Phone | ||
|---|---|---|---|---|
| Americas | Tom Goodman | Product Manager Low Voltage Products |
+1.732.795.4100, x4148 | tom.goodman@us.tdk-lambda.com |