- HOME
- News
- Press Releases
- Low Profile Power Supplies Require Less Space on DIN Rail
Low Profile Power Supplies Require Less Space on DIN Rail

San Diego, CA – December 2016 –
TDK Corporation announces the introduction of the TDK-Lambda brand DRL AC-DC DIN Rail mount power supplies. With efficiencies of up to 90%, waste heat has been reduced, allowing the use of very narrow width package sizes ranging from 18mm for the 10W, to 72mm for the 100W model. Less space on the rail provides additional room for other components or the use of smaller enclosures. The DRL series is suitable for a wide range of industrial applications including building and factory automation, security, process control and test and measurement.
The DRL series has an operating input range of 85 to 264Vac, and can withstand 300Vac for 5 seconds. The units have a Class II construction (double insulation) and do not require an earth ground connection. Input to output isolation is 3,000Vac. Four power levels and case sizes are offered - 10W, 30W, 60W and 100W – with a 24V output in all package sizes and a 12V output for the 10 to 60W versions. The 30 to 100W models have user adjustable outputs from either 12V to 15V or 24V to 28V.
The convection cooled units can operate in ambient temperatures from -20 to +71oC with derating applying at high temperatures. The DRLs are housed in a robust plastic case and share a common depth of 55.6mm and a height of 91mm. The 10 and 30W have an off-load power draw of <0.3W with the 60 and 100W at <0.5W.
All models certified to UL/CSA 60950-1, IEC/EN 60950-1 and UL 508 with CE marking for the Low Voltage, EMC and RoHS2 Directives. Select models also comply with NEC Class 2 in accordance with UL 1310. All units meet EN55011/EN55022-B conducted emissions (Class A radiated) and comply with IEC 61000-3-2 harmonics and IEC 61000-4 immunity standards.
More information and product availability can be obtained on the TDK Product Center, or by calling 800-LAMBDA-4.
Major applications
Building and factory automation, security, process control, test and measurement equipment
Main features and benefits
- Very narrow width
- Class II double insulated
- Class 2 operation in accordance with UL1310 (select models)
- Low off-load power consumption
Major specifications

About TDK Corporation
TDK Corporation is a leading electronics company based in Tokyo, Japan. It was established in 1935 to commercialize ferrite, a key material in electronic and magnetic products. TDK's portfolio includes electronic components, modules and systems* marketed under the product brands TDK and EPCOS, power supplies, magnetic application products as well as energy devices, flash memory application devices, and others. TDK focuses on demanding markets in the areas of information and communication technology and consumer, automotive and industrial electronics. The company has a network of design and manufacturing locations and sales offices in Asia, Europe, and in North and South America. In fiscal 2016, TDK posted total sales of USD 10.2 billion and employed about 92,000 people worldwide.
* The product portfolio includes ceramic, aluminum electrolytic and film capacitors, ferrites, inductors, high-frequency components such as surface acoustic wave (SAW) filter products and modules, piezo and protection components, and sensors.
About TDK-Lambda Corporation
TDK-Lambda Corporation, a group company of TDK Corporation, is a leading global power supply company providing highly reliable power supplies for industrial equipment worldwide. TDK-Lambda Corporation meets the various needs of customers with our entire range of activities, from research and development through to manufacturing, sales, and service with bases in five key areas, covering Japan, Europe, America, China, and Asia.
For more details, please pay a visit to http://www.tdk-lambda.com/
Downloads
Editorial Contact:
Tom Tillman, Director of Marketing
TDK-Lambda Americas Inc.
401 Mile of Cars Way, Suite 325
National City, CA 91950
Ph: 619-575-4400
Email: tom.tillman@us.tdk-lambda.com