- HOME
- News
- Press Releases
- 3200W Industrial Power Supply Has 400/440/480V 3-Phase Delta or Wye AC Input
3200W Industrial Power Supply Has 400/440/480V 3-Phase Delta or Wye AC Input
San Diego, CA – November 2016 –
TDK Corporation announces the introduction of the TDK-Lambda brand TPS3000-24 power supply. Delivering up to 3200W output power (24V at 133.3A) in a 2U high package, the TPS will operate from a wide range Delta or Wye 350 - 528Vac three phase input. This industrial power supply is ideal for use in many applications including test and measurement equipment, semiconductor fabrication, printers, lasers and RF power amplifiers. The high voltage, three-phase input avoids the requirement for step down transformers and assists phase load current balancing.
The TPS3000 is fully featured with isolated AC Fail, DC Good and dropped phase signals, remote on/off, remote sense and a 12V 0.3A standby supply. A PMBus™ communications interface allows remote monitoring of the output voltage, output current, internal temperature, status signals and fan speed. In addition, the output voltage, over current limit and the remote on/off can be programmed by the PMBus™. The output voltage can also be adjusted from 19.2 – 29V and the current limit point by 70-105% using front panel potentiometers or an analog 0-5Vdc voltage. Up to eight units can be connected in parallel for higher power and internal ORing FETs allow redundant operation.
The 92% efficient unit can operate at full load in ambient temperatures of up to 50oC, and deliver up to 55% load at 70oC. Cooling is provided by an internal temperature controlled fan to reduce acoustical noise. The case measures 107 x 84.4 x 324mm, making it suitable for 2U high racking systems and the weight is just 2.7kg.
The power supply has 3kVac input to output, 2kVac input to ground and 500Vac output to ground isolation with all models certified to UL/CSA 60950-1, IEC/EN 60950-1 and carrying the CE mark for the Low Voltage and RoHS2 Directives. The TPS3000-24 complies with EN55022-A conducted and radiated emissions, and meets the IEC 61000-3-2 harmonics, IEC 61000-4 immunity and SEMI F47-0706 standards.
More information and product availability can be obtained on the TDK Product Center, or by calling 800-LAMBDA-4.
Major applications
Test and measurement equipment, semiconductor fabrication, printers, lasers, RF power amplifiers.
Main features and benefits
- Suitable for 400/440/480Vac 3-phase Delta and Wye inputs
- Compact 2U high package size
- Fully featured
- 92% efficient
- PMBus™ communications interface for remote programming and monitoring
Major specifications

About TDK Corporation
TDK Corporation is a leading electronics company based in Tokyo, Japan. It was established in 1935 to commercialize ferrite, a key material in electronic and magnetic products. TDK's portfolio includes electronic components, modules and systems* marketed under the product brands TDK and EPCOS, power supplies, magnetic application products as well as energy devices, flash memory application devices, and others. TDK focuses on demanding markets in the areas of information and communication technology and consumer, automotive and industrial electronics. The company has a network of design and manufacturing locations and sales offices in Asia, Europe, and in North and South America. In fiscal 2016, TDK posted total sales of USD 10.2 billion and employed about 92,000 people worldwide.
* The product portfolio includes ceramic, aluminum electrolytic and film capacitors, ferrites, inductors, high-frequency components such as surface acoustic wave (SAW) filter products and modules, piezo and protection components, and sensors.
About TDK-Lambda
TDK Corporation is a leading electronics company based in Tokyo, Japan. It was established in 1935 to commercialize ferrite, a key material in electronic and magnetic products. TDK's portfolio includes electronic components, modules and systems* marketed under the product brands TDK and EPCOS, power supplies, magnetic application products as well as energy devices, flash memory application devices, and others. TDK focuses on demanding markets in the areas of information and communication technology and consumer, automotive and industrial electronics. The company has a network of design and manufacturing locations and sales offices in Asia, Europe, and in North and South America. In fiscal 2016, TDK posted total sales of USD 10.2 billion and employed about 92,000 people worldwide.
* The product portfolio includes ceramic, aluminum electrolytic and film capacitors, ferrites, inductors, high-frequency components such as surface acoustic wave (SAW) filter products and modules, piezo and protection components, and sensors.
Downloads
Editorial Contact:
Tom Tillman, Director of Marketing
TDK-Lambda Americas Inc.
401 Mile of Cars Way, Suite 325
National City, CA 91950
Ph: 619-575-4400
Email: tom.tillman@us.tdk-lambda.com